990-66230A-001

Shut Down a Single UPS

  1. Open BB.
    Wait approximately 10 seconds and the mimic diagram is shown on the display.
  2. Open UIB.

    Wait approximately 1 second and the UPS transfers to static bypass operation mode.

  3. Open SSIB.
    The UPS display turns off and the UPS shuts down.
  4. Open UOB.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?