990-66230A-001

Configure the Input Contacts

  1. From the main menu, tap Configuration > Contacts and relays and select the input contact that you want to configure.
  2. Select a function from the drop-down list for the selected input contact:
    Generator input: The generator has been connected with the system. Alarm cleared: The alarm is cleared.
    MBB contact NO: The maintenance bypass disconnect device MBB is closed (normally open contacts). Battery over charge: The battery is overcharged and charging is prohibited.
    Mute: The buzzer is muted. Battery over discharge: The battery is over discharged and discharging is prohibited
    BB status: Shows the status of the battery disconnect device. Electrolyte leakage: Indicates an electrolyte leakage.
    Transfer inverter: The UPS is transferred to inverter operation. MBB contact NC: The maintenance bypass disconnect device MBB is closed (normally closed contacts).
    BB online: The battery disconnect device is closed. Surge protection abnormal*
    Transfer bypass: The UPS is transferred to bypass operation. Turn off charger: The charger is turned off.
  3. On each page, tap OK to save your settings and tap the arrow symbol to go to the next page.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?