990-66230A-001

UPS Modes

Normal Operation

The UPS provides power to the connected load from mains. The UPS converts mains to conditioned power for the connected load while recharging the batteries (float or boost charge).

Battery Operation

The UPS transfers to battery operation if the mains supply fails. The UPS provides power to the connected load from the connected batteries for a finite period. When the mains supply returns, the UPS transfers back to normal operation.

Static Bypass Operation

The UPS supplies the load with power from the bypass source. If the conditions for normal or battery operation are not met, the load will be transferred from the inverter to the bypass source with no interruption in power to the load.

Maintenance Bypass Operation

In maintenance bypass operation, the mains is sent via the external or internal MBB to the load. Battery backup is not available in maintenance bypass operation.

ECO Mode

In ECO mode the UPS is configured to use static bypass operation as the preferred operation mode under predefined circumstances. The inverter is in standby in ECO mode and in case of interruption to the mains, the UPS transfers to battery operation and the load is supplied from the inverter.

NOTE: This mode is disabled by default, please contact Schneider Electric to enable this mode. If ECO mode is enabled, you cannot exit this operation mode by using the display, please also contact Schneider Electric for assistance.

OFF Mode

The UPS is not supplying the load with power. The batteries are charged and the display is on.

Frequency Converter Mode

In frequency converter mode, the UPS presents a stable output frequency (at 50 or 60 Hz) and static bypass is not available.
NOTICE
Risk of equipment damage or load drop
In frequency converter mode the UPS cannot run in static bypass operation or maintenance bypass operation. Before turning the UPS into frequency converter mode, you must contact a Schneider Electric-certified partner to make sure that:
  • the SSIB and the MBB are in the OFF (opened) position (Schneider Electric strongly recommends to lock these with a padlock available from Schneider Electric)
  • no cables are connected to the bypass terminals
Failure to follow these instructions can result in equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?