DUG_ELKO - Smart ZB Thermostat 16 A_WH-00

About the device

The Smart ZB Thermostat 16 A (hereinafter referred to as cFMT / thermostat) is mainly used to control the temperature in electrical heating applications like electrical underfloor heating and electrical radiators / heating panels.

Operating elements

  1. Dot-matrix display

    • Wireless connectivity LED ()

    • Heat demand LED ()

  2. Touch buttons

    • +/–: to increase / decrease the value.

    • O: function button

TIP: All LED indications are explained in the LED behavior chapter.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.