DUG_ELKO - Smart ZB Thermostat 16 A_WH-00

Pairing the device with the Wiser hub

Using the Wiser Home app, you can pair your thermostat with the Wiser Hub to access and control the thermostat.
To pair the thermostat:
  1. On the Home page, tap .
  2. Tap Devices > >Climate tab.
    TIP: You can also navigate by tapping Control tab > > Climate tab.
  3. Tap Flush Mount Thermostat and select the thermostat you want to pair.
  4. Tap Next
    The next screen shows the thermostat joining process.
  5. On thermostat press and hold the O touch button simultaneously (> 3 s) until Jn appears on the device.
    The wireless LED blinks amber when joining.
  6. Wait for a few seconds until the wireless LED on the thermostat turns green.
    NOTE: The wireless LED on the thermostat turns red if it is unable to connect.
    Upon successful pairing, the app displays the device joining status.
  7. Add a name for the thermostat and tap Next
  8. Assign a thermostat to the room and then tap Submit.

    After you pair the device, a success screen appears with the following options:

    • + Add New Device: Tap to continue pairing more devices.

    • Start Using Your Device: Tap to start using the paired device.

    NOTE: The success screen appears only if you are logged in as a Home Owner.

The thermostat is now listed on the Control tab under the All and the specific room tabs.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.