DUG_ELKO - Smart ZB Thermostat 16 A_WH-00

Configuring the device

IMPORTANT: The temperature data from the sensor will be used as an input for the heating system of the room. If a room has multiple temperature measuring devices (Room Thermostat, Smart ZB Thermostat 16A, or SmartSensor Climate Wireless), the system calculates the average temperature measured from the devices to control the heating based on the overall temperature of the room.
For more details, refer to the Setting the device as temperature source.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.