DUG_ELKO - Smart ZB Thermostat 16 A_WH-00

Installing the device

Refer to the installation instruction supplied with this product.

See Smart ZB Thermostat 16 A.

NOTE: It is strongly recommended to use a surge protection device in case thermostat is connected in the same circuit with inductive loads (e.g. fluorescent lights, Contactors or Motor Drives).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.