DUG_ELKO - Smart ZB Thermostat 16 A_WH-00

Setting the display brightness

Using the Wiser Home app, you can set the thermostat display brightness such as active (brightness during interaction) and inactive (brightness after 60 seconds of inactivity).
To set the thermostat display brightness:
  1. On the Home screen, tap .
  2. Tap Devices > Flush Mount Thermostat > Room settings > Brightness (A).
  3. Set the active and inactive brightness using the sliding bars.
    NOTE:
    • Default active screen brightness is 100%. Range from 1%~100%, and the setting accuracy is 1%.

    • Default inactive screen brightness is 0% range is 0%~100%, the setting accuracy is 1%, and it must be <= active brightness.

    For example:
    Allowed: Both active and inactive brightness can be set to 50%.

    Not allowed: Inactive brightness set to 60 % and active brightness set to 50 %.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.