DUG_ELKO - Smart ZB Thermostat 16 A_WH-00

Removing the device

Using the Wiser Home app, you can remove the thermostat from the Wiser system.
To remove the thermostat from the Wiser system:
  1. On the Home page, tap .
  2. Tap Devices > Flush Mount Thermostat > Room settings > Delete (A).
  3. Read the confirmation message and tap Ok to remove the thermostat from the Wiser system.
    NOTE: By removing the thermostat, you will reset the thermostat. If you still have a problem with the reset, then refer to resetting the device.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.