DUG_ELKO - Smart ZB Thermostat 16 A_WH-00

Advanced device settings

The Wiser Home app offers advanced settings for the thermostat. These settings include toggle switches that let you enable or disable valve protection, enable cooling input and output relay, and set cycle time and universal input.
NOTE: Making changes to advanced settings can severely impact your system, so be sure to understand its impact before applying any changes to the advanced settings.

To do advanced settings:
  1. On the Home screen, tap .
  2. Tap Devices > Flush Mount Thermostat > Room settings > Advanced Settings (A).
  3. Read the caution and tap OK.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.