DUG_ELKO - Smart ZB Thermostat 16 A_WH-00

Amazon Alexa™

Amazon Alexa™ (Alexa) is an intelligent personal assistant developed by Amazon™, and is capable of voice interaction.

Common Wiser commands for Alexa

  • Discover Devices: “Alexa, discover devices”

  • Reduce Temperature: “Alexa, decrease the temperature upstairs by 4 degrees”

  • Increase Temperature: “Alexa, increase the temperature upstairs by 3 degrees”

  • Set Temperature: “Alexa, set the upstairs to 20 degrees”

  • Get Temperature: “Alexa, what is the temperature upstairs?

  • Get the Setpoint: “Alexa, what is the upstairs set to?”


Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.