990-91375D-001

Connect the Signal Cables for GVBBB630EL-1CB to the Galaxy VS UPS

Recommended signal cable size Maximum distance to the UPS
0.5 mm2 50 meters
0.75 mm2 100 meters
1.0 mm2 200 meters
  1. Lockout/Tagout the battery breaker.
  2. Loosen the screws of the protection covers and lift the protection covers up and out of the battery breaker box.
  3. Remove the cover on the battery breaker.
  4. Route the signal cables through the bottom of the battery breaker box.
  5. Connect the signal cables:
    1. Connect the signal cables to the AUX switch.
    2. Connect the signal cables to the undervoltage trip coil.
    3. Fasten the signal cables with cable ties (provided) to the cable relief.
  6. Reinstall the cover on the battery breaker.
  7. Route the signal cables separately from the power cables.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?