990-91375D-001

Mount the Battery Breaker Box to the Wall

CAUTION
Risk of injury or equipment damage
  • Mount the battery breaker box to a wall or a rack that is structurally sound and able to support the weight of the unit.
  • Use appropriate hardware (not supplied) to mount the battery breaker box to the wall.
Failure to follow these instructions can result in injury or equipment damage.
NOTE: Four M10 x 30 torx and nuts are supplied for mounting the battery breaker box to a rack.

GVBBB630EL-1CB

GVBBB630EL-2CB and GVBBB630EL-3CB

  1. Measure and mark the four mounting hole locations on the wall.
  2. Drill holes in each of the four marked locations.
  3. Loosen the three screws and open the inner door.
  4. Mount the battery breaker box to the wall.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.