990-93888A-001

Connect the Signal Cables for External Synchronization

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Check for absence of voltage for all three signal terminals on the external synchronization board 0P4809. When the external synchronization cables are installed, the terminals on the external synchronization board 0P4809 may be energized. Disconnect the fuse disconnector device at the source before removing the transparent protection cover.
Failure to follow these instructions will result in death or serious injury.

Cable Size and Fuse Disconnector Device for External Synchronization

  Fuse and disconnector at source Fuse disconnector marking Cable size Conduits
IEC In = 2A, I.R=65 kAiC Fuse disconnector identification number and external synchronization UPS number. 2 x 1.5 mm2
UL/NEC 2 x 16 AWG 0.5 inch

The maximum voltage for external synchronization is equal to the input voltage range given in the specifications. The non-Class 2/non-SELV cables for external synchronization shall be a jacket cable and rated for 600 VAC.

  1. Remove the transparent protection cover from the external synchronization board 0P4809. The external synchronization board 0P4809 is located on the rear of the front plate.
  2. Connect the cables for external synchronization to the external synchronization board 0P4809 and to terminals J8309 and J8310. See cable routing on the illustration. Connect the external synchronization per your configuration according to one of the diagrams below. Ensure that fuse disconnector devices are installed at the source as shown in the diagrams.

    Signal Cable Connections for UPS Synchronization to a Fixed Voltage Source

    NOTE: The connection on J8309 pin 3 and 4 can be with a jumper or can be controlled externally from a PLC or another external system.

    Signal Cable Connections for Advanced Dual UPS Synchronization

    Signal Cable Connections for Advanced Dual UPS Synchronization in a Parallel UPS System with Fixed Sync Master

  3. Reinstall the transparent protection cover on the external synchronization board 0P4809 after signal cabling is completed.
    DANGER
    Hazard of electric shock, explosion, or arc flash
    The transparent protection cover must be installed over the external synchronization board 0P4809.
    Failure to follow these instructions will result in death or serious injury.
  4. Mark the transparent protection cover with the external synchronization fuse disconnector identification number.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?