990-93888A-001

Position the UPS

DANGER
Hazard of electric shock, explosion, or arc flash
The UPS must be secured against movement. Perform one of the following once the UPS is in its final position:
  • Lower the leveling feet until the casters no longer have contact with the floor, OR
  • Mount the front transportation bracket (870-32577) on the UPS to the floor.
Failure to follow these instructions will result in death or serious injury.
  1. Push the UPS into final position.
  2. Reinstall the front transportation bracket (870-32577) on the UPS.
  3. Perform one of the following:
    • Mount the front transportation bracket to the floor. Use appropriate hardware for the floor type.
    • Lower the front and rear leveling feet on the UPS with a wrench until they connect with the floor. The casters must not have contact with the floor. Use a bubble-leveler to check that the UPS is level.
      NOTICE
      Risk of equipment damage
      Do not move the cabinet after the leveling feet have been lowered.
      Failure to follow these instructions can result in equipment damage.
      NOTICE
      Risk of equipment damage
      Install the front transportation bracket to avoid the UPS overheating from circulating hot air from the rear outlets. The front transportation bracket blocks the hot air backflow.
      Failure to follow these instructions can result in equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?