Installation Procedure for UPS and Lithium-ion Battery Cabinets
DANGER |
|---|
|
Hazard of electric shock, explosion, or arc flash
The UPS must be secured against movement. Perform one
of the following once the UPS is in its final position:
Failure to follow these instructions will result in death or serious injury.
|
- Lithium-ion battery cabinet(s): Prepare for Installation.
- UPS: Perform one of the following procedures:
- Without seismic anchoring: Position the UPS.
- With seismic anchoring: Install the Seismic Anchoring and Position the UPS.
- Lithium-ion battery cabinet(s): Install the Rear Seismic Anchoring.
- Lithium-ion battery cabinet(s): Position and Interconnect the Battery Cabinets.
- Lithium-ion battery cabinet(s): Install the Front Seismic Anchoring.
- UPS: Perform one of the following procedures:
- Top cable entry: Prepare the UPS for Top Cable Entry.
- Bottom cable entry: Follow in the installation manual provided with the bottom entry cabinet.
- UPS: Only for TNC or HRG earthing system:
- UPS: Perform one of the following procedures:
- UPS: Connect the Signal Cables.
- UPS: Connect the Signal Cables from Switchgear and Third-Party Auxiliary Products.
- UPS: Connect the Modbus Cables.
- UPS: Only for external synchronization: Connect the Signal Cables for External Synchronization.
- UPS: Option: Install the ERMS Door Switch Kit GVLOPT011 (Option).
- UPS: Install the Power Module(s).
- UPS: Add Translated Safety Labels to Your Product.
- UPS: Final installation.
- Lithium-ion battery cabinet(s): Install the Battery Modules in the Battery Cabinet.
- Lithium-ion battery cabinet(s): Connect the Power Cables.
- Lithium-ion battery cabinet(s): Route the Signal Cables to the Switchgear, Rack BMS, and System BMS Ports.
DANGER |
|---|
|
hAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Startup must only be performed by Schneider Electric.
Failure to follow these instructions will result in death or serious injury.
|
For moving or decommissioning the UPS or the Lithium-ion battery cabinets after installation has been completed, see Decommission or Move the UPS to a New Location or Decommission or Move the Battery Cabinet to a New Location.


DANGER
DANGER