990-93888A-001

Install the Front Seismic Anchoring

  1. Install the front seismic bracket (front shipping bracket) on the battery cabinet.
  2. Anchor the front seismic bracket to the floor using appropriate hardware for the floor type – the hole diameter in the front seismic bracket is ø14 mm. The minimum requirement is M12 strength grade 8.8 hardware.
    NOTE: Floor anchoring bolts are not supplied.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?