990-93888A-001

Install the Seismic Anchoring and Position the UPS

Use the optional seismic kit GVLOPT002 for this procedure.

  1. Mount the rear anchoring assembly to the floor. Use appropriate hardware for the floor type – the hole diameter in the rear anchors is ø16 mm. Minimum requirement is M12 strength grade 8.8 hardware.

    Rear View

  2. Remove all the screws and remove the anchoring bracket.

    Rear View

  3. Install the rear anchoring brackets on the UPS with the provided M8x25 bolts.

    Rear View

  4. Push the UPS into final position. Align with the seismic anchoring.

    Rear View

  5. Install the seismic front anchoring bracket on the UPS and mount it to the floor. Use appropriate hardware for the floor type – the hole diameter in the bracket is ø9 mm. Minimum requirement is M8 strength grade 8.8 hardware.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?