990-93888A-001

Install the Power Module(s)

The UPS can arrive with or without preinstalled power modules. Additional power modules are shipped separately and must be installed to reach the correct UPS kW rating.
CAUTION
Heavy load
Power modules are heavy (38 kg (83.77 lbs)) and require two persons to lift.
Failure to follow these instructions can result in injury or equipment damage.
  1. Remove the filler plate from the empty power module slot. Save the filler plate for future use.
  2. Push the power module into the slot. The enable mechanism will latch when the power module is correctly inserted.
  3. Install the provided screws in the top and the bottom of the power module.
Install the power modules in the shown order from 1-10.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?