990-93888A-001

Prepare for TNC Earthing System

  1. Connect power cable(s) (not provided) from the PE busbar to the N busbar. Use the same number of cables and cable size as the output N cables.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?