990-93888A-001

Decommission or Move the UPS to a New Location

  1. Shut down the UPS completely – follow the instructions in the UPS operation manual.
  2. Lockout/Tagout all disconnect devices in the maintenance bypass cabinet/the switchgear in the OFF (open) position.
  3. Lockout/Tagout all battery disconnect devices in the switchgear/battery solution in the OFF (open) position.
  4. Open the front door of the UPS.
  5. If present, Lockout/Tagout the backfeed disconnect device BF2 in the OFF (open) position.
  6. Measure for and verify ABSENCE of voltage with a multimeter probe through the holes in the transparent plate for input, bypass, output, neutral, and DC.

    Front View of the UPS

  7. Remove all power modules from the top row of the UPS:
    WARNING
    Top-heavy cabinet
    Do not remove any power modules from the bottom row of the UPS. This will make the UPS top-heavy and make it tilt more easily.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.
    CAUTION
    Heavy load
    Power modules are heavy (38 kg (83.77 lbs)) and require two persons to lift.
    Failure to follow these instructions can result in injury or equipment damage.
    1. Remove the screws in the top and bottom of the power module and push the unlock switch.
    2. Pull the power module halfway out. A locking mechanism prevents the power module from being pulled all the way out.
    3. Release the lock by pressing the release button on the top of the power module and remove the power module.
    4. Install a filler plate (if available) in front of the empty power module slot.
    5. Store the power modules correctly until reinstallation.
      WARNING
      risk of equipment damage
      • Store the power modules at an ambient temperature of -15 to 40 °C (5 to 104 °F), 10-80% non-condensing humidity.
      • Store the power modules in their original protective packaging.
      Failure to follow these instructions can result in death, serious injury, or equipment damage.
  8. Open the inner door of the UPS.
  9. Measure for and verify ABSENCE of voltage on each input/bypass/output/neutral/DC busbar before continuing.
    DANGER
    hAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
    Measure for and verify ABSENCE of voltage on each input/bypass/output/neutral/DC busbar before continuing.
    Failure to follow these instructions will result in death or serious injury.
  10. For UPS system without maintenance bypass cabinet: Perform the following steps.
    1. Remove the transparent plastic protectors from the busbars. Remove the plastic box for easier access. Save all parts for reinstallation after cable disconnection.
      NOTE: On newer UPS models, the box (marked (C) on the illustration) is integrated in the inner door of the UPS instead of being a separate part. The integrated box must not be removed from the inner door.

      Front View of the UPS Model with Separate Plastic Box

      Front View of the UPS Model with the Box Integrated in the Inner Door

    2. Disconnect all power cables from the UPS.
    3. Reinstall the transparent plastic protectors (marked (A) on the illustration) and the plastic box (marked (B) on the illustration) in the original position.
      NOTE: On newer UPS models, the box (marked (C) on the illustration) is integrated in the inner door of the UPS instead of being a separate part.

      Front View of the UPS Model with Separate Plastic Box

      Front View of the UPS Model with the Box Integrated in the Inner Door

      CAUTION
      Risk of arc flash and overheating
      The transparent plastic protectors and the plastic box must be reinstalled in the original position after power cabling is completed. Note: On newer UPS models, the box is integrated in the inner door of the UPS instead of being a separate part.
      Failure to follow these instructions can result in injury or equipment damage.
  11. For UPS system with maintenance bypass cabinet: Remove the busbars and insulator parts that connect the UPS to the maintenance bypass cabinet. Refer to the maintenance bypass cabinet installation manual for details. Save all parts for reinstallation.

    Front View of the UPS

    Front View of the UPS

    Front View of the UPS

    Front View of the UPS

  12. For UPS system with maintenance bypass cabinet: Remove the top bracket and the screws in the front that interconnect the UPS and the maintenance bypass cabinet externally. Remove the two special screws that interconnect the UPS and the maintenance bypass cabinet internally. Refer to the maintenance bypass cabinet installation manual for details. Save all parts for reinstallation.

    Front View of the Maintenance Bypass Cabinet and the UPS

    Inside View of the Maintenance Bypass Cabinet and the UPS

  13. If external sync is present: Remove the transparent protection cover from the external synchronization board 0P4809. The external synchronization board 0P4809 is located on the rear of the front plate. Disconnect the signal cables from the external synchronization board 0P4809.
    DANGER
    HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
    Check for absence of voltage for all three signal terminals on the external synchronization board 0P4809. When the external synchronization cables are installed, the terminals on the external synchronization board 0P4809 may be energized. Disconnect the fuse disconnector device at the source before removing the transparent protection cover.
    Failure to follow these instructions will result in death or serious injury.
  14. Close the inner door and reinstall the screws.
  15. Disconnect and remove any signal cables from the UPS.
  16. Remove the seismic front anchoring bracket/front transportation bracket from the UPS. Save for reinstallation.
  17. Close and lock the front door.
  18. Raise the feet of the UPS until the casters have full contact with the floor.
  19. You can now move the UPS by rolling it over the floor on the casters.
    WARNING
    TIPPING hazard
    • The casters of the UPS are exclusively for transport on flat, even, hard, and horizontal surfaces.
    • The casters of the UPS are intended for transport over short distances (i.e. inside the same building).
    • Move at a slow pace and pay close attention on the floor conditions and the balance of the UPS.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.
  20. If present, remove the rear seismic anchoring bracket from the UPS and remove the seismic anchors from the floor. Save for reinstallation.

    Rear View

  21. For transport over longer distances or in conditions that are not suitable for the casters of the UPS: Open the front door, remove all power modules from the bottom row of the UPS, close and lock the front door.
    WARNING
    Top-heavy cabinet
    The UPS will be top-heavy with no power modules installed. Take appropriate precautions during handling and preparation for transport/shipment.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.
    CAUTION
    Heavy load
    Power modules are heavy (38 kg (83.77 lbs)) and require two persons to lift.
    Failure to follow these instructions can result in injury or equipment damage.
    WARNING
    risk of equipment damage
    • Store the power modules at an ambient temperature of -15 to 40 °C (5 to 104 °F), 10-80% non-condensing humidity.
    • Store the power modules in their original protective packaging.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.
    WARNING
    TIPPING hazard
    For transport over longer distances or in conditions that are not suitable for the casters of the UPS, ensure:
    • that personnel performing the transport have necessary skill and have received adequate training;
    • to use appropriate tools to safely lift and transport the UPS;
    • to protect the product against damage by using appropriate protection (like wrapping or packaging).
    Failure to follow these instructions can result in death, serious injury, or equipment damage.

    Transportation requirements:

    • Mount the UPS in a vertical position in the center of a suitable pallet with minimum pallet dimensions: 1000 mm x 1150 mm (39.4 in x 45.3 in)). The pallet must be suitable for the weight of the UPS (400 kg (882 lbs) with no power modules installed).

    • Use appropriate means of fixation to mount the UPS to the pallet.

    • The original shipping pallet in combination with the original transportation brackets can be reused, if in undamaged condition.

    DANGER
    TIPPING hazard
    • The UPS must be appropriately fixed to the pallet immediately after being placed on the pallet.
    • The fixation hardware must be strong enough to withstand vibrations and shocks during loading, transport, and unloading.
    Failure to follow these instructions will result in death or serious injury.
    WARNING
    Unexpected equipment behavior
    Do not lift the UPS with a forklift/pallet truck directly on the frame as it may bend or damage the frame.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.
  22. Perform one of the following:
    • Decommission the UPS, OR
    • Move the UPS to a new location to install it.
  23. Only for installing the UPS in a new location: Follow the installation manual to install the UPS in the new location. See Installation Procedure for UPS and Lithium-ion Battery Cabinets or Installation Procedure for UPS with Maintenance Bypass Cabinet and Lithium-ion Battery Cabinets for installation overview. Startup must only be performed by Schneider Electric.
    DANGER
    hAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
    Startup must only be performed by Schneider Electric.
    Failure to follow these instructions will result in death or serious injury.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?