990-91317H-001

Galaxy VSUPS with Internal BatteriesTechnical Specifications

10-100 kW 400 V

Latest updates are available on the Schneider Electric website

5/2025

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?