990-91317H-001

Regional Seismic Compliance

Certificate available upon request.

Country/Region Code ID Hazard level ground Hazard level roof
Argentina INPRES-CIRSOC103 Zone 4 Zone 4
Australia AS 1170.4-2007 Z = 0.22 Z = 0.22
Canada* 2020 NBCC Sa = 2.0 Sa = 1.46
Chile NCh 433.Of1996 Zone 3 Zone 2
China GB 50011-2010 (2016) αMax = 1.4 αMax = 1.2
Europe Eurocode 8 EN1998-1 αgR = 0.45 αgR = 0.3
India IS 1893 (Part 1) : 2016 Z = 0.36 Z = 0.36
Japan Building Standard Law Zone A Zone A
New Zealand NZS 1170.5:2004+A1 Z = 0.6 Z = 0.42
Peru N.T.E. - E.030 Zone 4 Zone 4
Russia SNIP II-7-81 (SP 14.13330.2014) MSK 10 MSK 9
Taiwan CPA 2011 Seismic Design Code SSD = 0.8 SSD = 0.8
U.S.A.* ASCE 7-16 / IBC 2018 SDS = 2.0 SDS = 1.47
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?