990-91317E-001

Single System Overview

UIB Unit input breaker
SSIB Static switch input breaker
IMB Internal maintenance breaker
UOB Unit output breaker
BB Battery breaker in UPS for internal batteries and in external battery solution (if present)

Single System – Single Mains

Single System – Dual Mains

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?