990-91317H-001

Drawings

NOTE: A comprehensive set of drawings is available on www.se.com.
NOTE: These drawings are for reference ONLY – subject to change without notice.

10-20 kW 400 V

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?