990-91284-001

Final Installation

  1. Reinstall the plates on the maintenance bypass cabinet:
    1. Reinstall the lower transparent plate.
    2. Reinstall the upper transparent plate.
    3. Reinstall the lower front plate.
    4. Reinstall the middle front plate.
    5. Reinstall the upper front plate.

    Front View of the Maintenance Bypass Cabinet

  2. Only for seismic anchoring:
    1. Install the seismic front anchoring bracket on the maintenance bypass cabinet with the provided M8 bolts.
    2. Mount the seismic front anchoring bracket on the maintenance bypass cabinet to the floor. Use appropriate hardware for the floor type – the hole diameter in the front anchoring bracket is ø18 mm.

    Front View of the Maintenance Bypass Cabinet

  3. Reinstall the front panel on the maintenance bypass cabinet:
    1. Insert the two tabs in the bottom of the front panel in the maintenance bypass cabinet at a tilted angle.
    2. Reconnect the front panel strap to the maintenance bypass cabinet.
    3. Close the front panel and lock with the two locking knobs.

      Front Right View of the Maintenance Bypass Cabinet

  4. Follow the UPS installation manual to connect the power cables from the maintenance bypass cabinet in the UPS and to complete the rest of the UPS installation.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?