990-91284-001

Install Conduit Box and Connect Power Cables Between the UPS and the Maintenance Bypass Cabinet

  1. Remove the upper and middle rear plates from the UPS.

    Rear View of the Maintenance Bypass Cabinet

  2. Remove the rear plate from the conduit box.
  3. Install the conduit box on the maintenance bypass cabinet with the provided screws.

    Rear View of the Maintenance Bypass Cabinet

  4. Install the provided conduits in the bottom of the conduit box.
  5. Route the provided UPS input cables and UPS output cables through the bottom of the conduit box and through the side brackets as shown. Note that the PE from the UPS input cables is routed with the UPS output cables.
  6. Connect the UPS output cables to the PE busbar, UOB, and the N busbar.
  7. Connect the UPS input cables to the PE busbar and UIB.
  8. Reinstall the rear plate on the conduit box.
  9. Reinstall the upper rear plate on the maintenance bypass cabinet.
  10. When the UPS has been installed, the UPS input cables and the UPS output cables must be routed in through the conduit box on the UPS. Follow the UPS installation manual to connect the power cables from the maintenance bypass cabinet in the UPS.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.