990-91284-001

Prepare the Maintenance Bypass Cabinet for Cables

  1. Remove the front panel from the maintenance bypass cabinet.
  2. Remove the top cover from the maintenance bypass cabinet.
  3. Remove the lower, middle, and upper front plates from the maintenance bypass cabinet.
  4. Remove the transparent plates from the maintenance bypass cabinet.
  5. Remove the right side panel from the UPS and reinstall the side panel on the right side of the maintenance bypass cabinet.
  6. Remove the gland plate from the top or bottom of the maintenance bypass cabinet.
  7. Drill or punch holes for power cables or conduits in the gland plate. Conduits are not provided.
    DANGER
    Hazard of electric shock, explosion, or arc flash
    Do not drill or cut holes for power cables or conduits with the gland plate installed and do not drill or cut holes in close proximity to the maintenance bypass cabinet.
    Failure to follow these instructions will result in death or serious injury.
  8. Reinstall the gland plate in the top cover or in the bottom of the maintenance bypass cabinet.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?