990-91284-001

Installation Procedure

Top Entry Installation without Conduit Box

Top Entry Installation with Conduit Box

 

Bottom Entry Installation

  1. Follow the UPS manual to prepare the UPS for installation.
  2. Prepare the Maintenance Bypass Cabinet for Cables.
  3. Perform one of the following:
  4. Install the Seismic Anchoring (Option).
  5. Interconnect the UPS and the Maintenance Bypass Cabinet.
  6. Perform one of the following:
  7. Connect the Signal Cables.
  8. Final Installation.
  9. Follow the UPS installation manual to connect the power cables from the maintenance bypass cabinet in the UPS and to complete the rest of the UPS installation.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?