990-91284-001

Interconnect the UPS and the Maintenance Bypass Cabinet

  1. Reinstall the top cover on the maintenance bypass cabinet with four screws.
  2. Remove the three interconnection screws from the left side of the maintenance bypass cabinet. Save for interconnection.
  3. Push the UPS into place up against the maintenance bypass cabinet. The rear bracket on the maintenance bypass cabinet must connect to the UPS.

    Rear View of the Maintenance Bypass Cabinet and the UPS

  4. Install the three interconnection screws between the UPS and the maintenance bypass cabinet as shown.

    Front View of the UPS and the Maintenance Bypass Cabinet

  5. Lower the front and rear leveling feet on the UPS and the maintenance bypass cabinet with a wrench until they connect with the floor. Use a bubble-leveler to check that the UPS and maintenance bypass cabinet are level.

    Front View of the UPS

    NOTICE
    Risk of Equipment damage
    Do not move the cabinet after the leveling feet have been lowered.
    Failure to follow these instructions can result in equipment damage.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.