990-91284-001

Install the Seismic Anchoring (Option)

Use the optional installation kits GVSOPT002 (shipped with the UPS) and GVSOPT008 for this procedure.
  1. Interconnect the rear anchors for the UPS and the maintenance bypass cabinet with the interconnection plate and four M8 bolts (provided).
  2. Mount the rear anchor assembly to the floor. Use appropriate hardware for the floor type – the hole diameter in the rear anchor is ø14 mm.
  3. Install the rear anchoring brackets on the UPS and the maintenance bypass cabinet with the M8 bolts (provided).

    Rear View of the Maintenance Bypass Cabinet

  4. Push the maintenance bypass cabinet into position so the rear anchoring bracket connects to the rear anchor. The front anchoring bracket is installed in the final installation steps.
    NOTE: Do not push the UPS into position yet.

    Rear View of the Maintenance Bypass Cabinet

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.