990-91284-001

Maintenance Bypass Cabinet with Transformer Weights and Dimensions

Commercial reference Weight kg (lbs) Height mm (in) Width mm (in) Depth mm (in)
GVSBPIT25B 395 (870.83) 1485 (58.46) 600 (23.62) 836 (32.91)
GVSBPOT50B 530 (1168.45) 1485 (58.46) 600 (23.62) 836 (32.91)
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.