990-91284-001

Connect the Power Cables in a Maintenance Bypass Cabinet with Input Transformer

NOTE: Route the power cables in front of the horizontal bracket in the top or bottom of the maintenance bypass cabinet to ensure correct separation from the transformer.
  1. Perform one of the following:
    • For 480 V input transformer: Route the input cables through the top or bottom of the maintenance bypass cabinet and connect the input cables to the PE busbar and the upper 480 V input busbars.
    • For 600 V input transformer: Route the input cables through the top or bottom of the maintenance bypass cabinet and connect the input cables to the PE busbar and the lower 600 V input busbars.

    Front View of Maintenance Bypass Cabinet with Input Transformer

  2. Route the load cables through the top or bottom of the maintenance bypass cabinet and connect to the PE busbar, the load busbars, and the N busbar.
  3. Perform one of the following:
    • For top cable entry on a UPS without conduit box: Route the DC cables through the top of the maintenance bypass cabinet and connect to the PE busbar and the DC busbars.
    • All others: Follow the UPS installation manual to connect the DC cables directly in the UPS.
  4. Fasten the power cables to the horizontal bracket in the top or bottom of the maintenance bypass cabinet with cable ties.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.