Configure High Efficiency Mode
The UPS returns to high efficiency mode after 10 seconds under normal operating conditions. If an unstable mains forces the UPS to exit high efficiency mode more than one to ten times (this setting must be configured by Schneider Electric) within 24 hours, the UPS will disable high efficiency mode. An informational alarm will be generated, and Disabled by system will be shown on the screen . High efficiency must then be manually reactivated.
- From the home screen on the display select and configure
the following settings:
- Select High Efficiency Mode: Choose between Disable, ECO Mode, eConversion, and eConversion Harmonics Compensator.
- Tap > and configure the schedule
settings:
- Schedule: Select when the system should enter the selected eConversion or ECO mode. Choose between Always, Programmed and Never.
- Active Schedules List: If you chose Programmed above, select Enable and set the time and date for when the system should enter the selected eConversion or ECO mode.
- Tap OK to confirm your settings.