View the System Status Information
- From the home screen on the display select Status.
- Select the area for which you wish to see the status. Choose
between:
Input
Voltage (phase-to-neutral)*
The present phase-to-neutral input voltage in volts (V).
Current
The present input current from the AC utility power source per phase in amperes (A).
Maximum RMS Current
The maximum current for the latest 30 days.
Apparent Power
The present apparent power input for each phase in kVA. Apparent power is the product of RMS (root mean square) volts and RMS amperes.
Active Power
The present active power (or real power) input for each phase in kilowatts (kW). Active power is the portion of power flow that, averaged over a complete cycle of the AC waveform, results in net transfer of energy in one direction.
Power Factor
The ratio of the active power to apparent power.
Voltage (phase-to-phase)
The present phase-to-phase input voltage.
Total Apparent Power
The present total apparent power input (for all three phases) in kVA.
Total Active Power
The present total active power input (for all three phases) in kW.
Frequency
The present input frequency in hertz (Hz).
Energy
The total energy consumption since the time of installation or since the number was reset.
Output
Voltage (phase-to-neutral)*
The phase-to-neutral output voltage at the inverter in volts (V).
Current
The present output current for each phase in amperes (A).
Maximum RMS Current
The maximum current for the latest 30 days.
Apparent Power
The present apparent power output for each phase in kVA. Apparent power is the product of RMS (root mean square) volts and RMS amperes.
Active Power
The present active power (or real power) output for each phase in kilowatts (kW). Active power is the portion of power flow that, averaged over a complete cycle of the AC waveform, results in net transfer of energy in one direction.
Power Factor
The present output power factor for each phase. Power factor is the ratio of active power to apparent power.
Current Crest Factor
The present output crest factor for each phase. The output crest factor is the ratio of the peak value of the output current to the RMS (root mean square) value.
Current THD
The THD (total harmonic distortion) for each phase, as a percentage, for the present output current.
Voltage (phase-to-phase)
The phase-to-phase output voltage at the inverter in volts (V).
Total Apparent Power
The present apparent power output for each phase in thousands of Volt-Amps (kVA). Apparent power is the product of RMS (root mean square) volts and RMS amperes.
Total Active Power
The present total active output power (for all three phases) in kilowatts (kW).
Load
The percentage of the UPS capacity presently used across all phases. The load percentage for the highest phase load is displayed.
Neutral Current*
The present output neutral current in amperes (A).
Frequency
The present output frequency in hertz (Hz).
Inverter Status
The general condition of the inverter.
PFC Status
The general condition of the PFC.
Energy
The total energy supplied since the time of installation or since the value was reset.
Bypass
Voltage (phase-to-neutral)*
The present phase-to-neutral bypass voltage (V).
Current
The present bypass current for each phase, in amperes (A).
Maximum RMS Current
The maximum current for the latest 30 days.
Apparent Power
The present apparent bypass power for each phase in kVA. Apparent power is the product of RMS (root mean square) volts and RMS amperes.
Active Power
The present active bypass power for each phase in kilowatts (kW). Active power is the time average of the instantaneous product of voltage and current.
Power Factor
The present bypass power factor for each phase. Power factor is the ratio of active power to apparent power.
Voltage (phase-to-phase)
The present phase-to-phase bypass voltage (V).
Total Apparent Power
The present total apparent bypass power (for all three phases) in thousands of Volt-Amps (kVA).
Total Active Power
The present total active bypass power (for all three phases) in kilowatts (kW).
Frequency
The present bypass frequency in hertz (Hz).
Battery
Voltage
The present battery voltage.
Current
The present battery current in amperes (A).
A positive current indicates that the battery is charging; a negative current indicates that the battery is discharging.
Power
The present DC power being drawn from the battery, in kilowatts (kW).
Estimated Charge Level
The present battery charge, as a percentage of full charge capacity.
Estimated Charge Time
The estimated time, in minutes, until the batteries reach 100% charge.
Runtime Remaining
The amount of time in hours and minutes before the batteries reach the low-voltage shutdown level. Charger Mode
The operation mode of the charger (Off, Float, Boost, Equalization, Cyclic, Test).
Battery Status
The general condition of the battery.
Charger Status
The general condition of the charger.
Total Battery Capacity
The total capacity available from the available batteries.
Temperature
The highest battery temperature from the connected temperature sensors.
Temperature
Ambient Temperature
Ambient temperature in degrees Celsius or Fahrenheit for the I/O cabinet and each power cabinet.
System
Output Voltage
The phase-to-phase output voltage at the inverter in volts (V).
Output Current
The present output current for each phase in amperes (A).
Output Frequency
The present output frequency in hertz (Hz).
Runtime Remaining
The amount of time in hours and minutes before the batteries reach the low-voltage shutdown level.
System Time
The time of the UPS system.
UPS Operation Mode
The operation mode of the operated UPS.
System Operation Mode
The operation mode of the complete UPS system.
Total Output Power
The apparent and active power (or real power) output for each phase.
Overload Timer*
The time in seconds before the UPS changes to forced static bypass due to an overload condition on the system.
NOTE: The system can be in an overload condition even though the Total Output Power is below 100% if the load is not equally shared between the three phases.Output Power
The phase-to-phase apparent and active power (or real power) output for each phase.
Parallel System
Input Current
The present phase-to-phase input current in amperes (A).
Output Current
The present phase-to-phase output current in amperes (A).
Bypass Current
The present phase-to-phase bypass current in amperes (A).
Parallel UPS Number
The parallel UPS number of the operated UPS.
Parallel system redundancy
The redundancy for the parallel system.
Number of Parallel Units
The total number of UPSs in the parallel system.
Parallel Units
The numbers of all UPSs in the parallel system.
Output Total Apparent Power
The present total apparent output power (for all three phases) in thousands of Volt-Amps (kVA).
Output Total Load
The percentage of the UPS system capacity presently used across all phases. The load percentage for the highest phase load is displayed.
Active Alarms
Active Alarms
For more information on active alarms, go to View the Active Alarms.
Mimic Diagram
Mimic Diagram
The mimic diagram shows the current status of the main parts of the UPS system: power sources, converters, bypass static switch and breakers, and it shows the power flow through the system.
Detailed View
Detailed view
The detailed view shows the system with a status icon on each individual power cabinet and the actual number of redundant power cabinets. The detailed view also shows the apparent power and active power per phase.
Symbols on the Detailed View Screen
Peak Shaving Mode
Peak shaving mode
The status of the peak shaving mode — Active or Inactive
Input power
The present input power (kW).
Battery power
The present battery power (kW). The bar is green when the batteries are charging and yellow when the batteries are discharging.
Peak shaving
Indicates if the charger is enabled or disabled and if forced battery operation is enabled or disabled.
State of charge
The current charge status of the batteries.
Remaining time
The remaining time in battery operation and peak shaving mode.
- Tap the home button to exit the screens and return to the home screen.