990-914303-001

Shut Down System Operating as Frequency Converters

Use this procedure to shut down a single system, a parallel system operating as frequency converters.

NOTE: Only operate a breaker when the associated breaker LED is green.
  1. From the home screen on the display, select Control > Shutdown Wizard. Select Shutdown ending in Off Operation and follow the steps which appear on the screen.
    NOTE: The following is a generic shutdown procedure. Always follow the steps of the Shutdown Wizard which are specific to your system.
  2. Open the unit output breaker UOB.
  3. Open battery breakers (if present).
  4. Open the unit input breaker UIB.
  5. Repeat steps 1 to 4 on each Galaxy VX in the parallel system.
  6. Open the system isolation breaker (if present).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?