990-914303-001

Configure the Network

The network can be configured for the display and for the cards in Smart Slot 1 and Smart Slot 2.

  1. From the home screen on the display select Configuration > Network and select either Display, Smart Slot 1, or Smart Slot 2 if present.
  2. Configure the following settings:
    1. TCP/IPv4: Enable IPv4 (if applicable), and select the Address Mode (Manual, DCHP, or BOOTP).
    2. TCP/IPv6: Enable IPv6 (if applicable), select Auto Configuration or Manual Configuration, and select the DHCPv6 Mode (Router controlled, Non-Address Information Only, Never, or Address and Other Information).
      NOTE: Tap Addresses to see all valid IPv6 addresses.
    3. Web Access: Enable Web (if applicable) and select the Access Mode (HTTP or HTTPS).
      NOTE: Not available for Smart Slots.
    4. FTP server: Enable FTP (if applicable).
      NOTE: Not available for Smart Slots.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?