990-914303-001

Overview of UPS User Interface

Display Model 1

Display Model 2

  1. Display*

  2. Status LEDs

  3. Mimic diagram

  4. Inverter ON button

  5. Inverter OFF button

  6. USB port for export of logs

  7. Display reboot button

  8. Network connection LED:

    • Solid green: The system has valid TCP/IP settings.

      See Configure the Network.

    • Flashing green: The system does not have valid TCP/IP settings.

    • Solid orange: The display is inoperable. Contact Schneider Electric.

    • Flashing orange: The system is making BOOTP requests.

      See Configure the Network.

    • Alternately flashing green and orange: If the LED is alternately flashing slowly, the system is making DHCP requests.

      See Configure the Network.

      If the LED is alternately flashing rapidly, the system is starting up.

    • Off: The display is not receiving input power or the display is inoperable.

  9. LED for indication of network connection type:

    • Solid green: The system is connected to a network operating at 10 Megabits per second (Mbps).

    • Flashing green: The system is receiving or transmitting data packets at 10 Megabits per second (Mbps).

    • Solid orange: The system is connected to a network operating at 100 Megabits per second (Mbps).

    • Flashing orange: The system is receiving or transmitting data packets at 100 Megabits per second (Mbps).

    • Off: One or more of the following exists: The display is not receiving input power, the cable that connects the system to the network is disconnected, the device that connects the system to the network is turned off, or the display is inoperable. Check the connections and if the LED remains off, contact Schneider Electric.

  10. Reserved for service.

Overview of Mimic Diagram

The mimic diagram shows the power flow through the UPS system, and the status of the main functions.

Each LED can be in one of the below three states:

Green

The corresponding function is active and OK

Red

The corresponding function is not working properly

Off

The corresponding function is not active

Overview of Status LEDs

The status LEDs placed next to the display show the current status of the UPS system:

Display Model 1 – LED symbols Display Model 2 – LED symbols LED color LED description
Green
  • Green LED on: The load is protected

  • Green LED + orange LED on: The load is protected, but the system reports an alarm at warning level

  • Orange LED + red LED on: The load is unprotected and the system reports an alarm at warning level and an alarm at critical level

  • Red on: The load is unprotected and the system reports an alarm at critical level

Yellow
Red

Display Symbols

Symbol

Description

The locked home button appears when the system is locked by a password protection. Tap this button to go to the home screen of the display.

The unlocked home button appears when the system has been unlocked using the password. Tap this button to go to the home screen of the display.

Tap the OK button to confirm your selections and exit the current screen.

Tap the ESC button to cancel your changes and exit the current screen.

Tap the filter button to set up the filters for your logs.

Tap the recycle bin button to clear the log.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?