990-914303-001

Configure the UPS Output Voltage Compensation

  1. From the home screen on the display select Configuration > UPS > Output.
  2. Tap arrow to the right to go to the next output configuration screen.
  3. Under Voltage Compensation select the preferred voltage compensation for your system. Choose between –3%, –2%, –1%, 0%, 1%, 2%, or 3%.
    NOTE: This setting is shared between all UPSs in a parallel system.
  4. Under Output Voltage Compensation with Loaded Transformer select the preferred output voltage compensation to compensate for load dependent transformer voltage drop. Choose between 0%, 1%, 2%, or 3%.
    NOTE: This setting must be identical for all UPSs in a parallel system.
    NOTE: When this setting is set to 0%, the output transformer voltage compensation is disabled.
  5. Tap OK to confirm your setting.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?