990-914303-001

Restart the Battery Solution

  1. Perform the following steps on all battery cabinets in the battery solution.
    1. Remove the cover in front of the start-up button and push the start-up button.
      • The PSU2 LED and the POWER LED will turn on.

      • The ABNORMAL and ALARM LEDs should remain off.

    2. Reinstall the cover in front of the start-up button.
    3. Set the battery breaker to the ON (closed) position.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?