990-914303-001

Reboot the Display

NOTE: A reboot of the display does not impact the settings made.
  1. Open the shutter door on the front right side of the display.
  2. Press the reboot button (A) with a pointed object like a pen or a paper clip.

    Display Model 1

    Display Model 2

    The display is rebooted.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?