990-914303-001

Isolate this Single UPS from the Parallel System

Use this procedure to shut down one UPS in a running parallel system.

NOTE: Before initiating this procedure, ensure that the remaining UPS units can supply the load.
NOTE: Only operate a breaker when the associated breaker LED is green.
  1. From the home screen on the display, select Control > Shutdown Wizard. Select Shut down UPS in a parallel system and follow the steps which appear on the screen.
    NOTE: The following is a generic shutdown procedure. Always follow the steps of the Shutdown Wizard which are specific to your system.
  2. Turn off the UPS by pressing the Inverter OFF key on the front of the UPS.
  3. Open the unit output breaker UOB.
  4. Open the static switch input breaker SSIB.
  5. Open the battery breakers in your specific battery solution.
  6. Open the unit input breaker UIB.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?