990-914303-001

Configure the Modbus

The modbus can be configured for the display and for the cards in Smart Slot 1 and Smart Slot 2.

NOTE: Only the display and optional Network Management Card AP9635 can be used for serial modbus.
  1. From the home screen on the display select Configuration > Modbus and select either Display, Smart Slot 1, or Smart Slot 2.
  2. Configure the modbus by enabling Serial or TCP access, and adding the needed values.
  3. Tap OK to confirm your settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?