Operation Modes
The Galaxy UPS has two different levels of operation mode:
-
UPS Operation Mode: The operation mode of the operated UPS. See UPS Modes.
-
System Operation Mode: The operation mode of the complete UPS system. See System Modes.
UPS Modes
eConversion Mode
eConversion provides a combination of maximum protection and highest efficiency, that permits to reduce the electricity absorbed by the UPS by a factor three compared with double conversion. eConversion is now the generally recommended operation mode and is enabled by default in the UPS but it can be disabled via the display menu. When enabled, eConversion can be set to always active or on a set schedule configured through the display menu.
In eConversion the UPS supplies the active part of the load through the static bypass as long as the utility/mains supply is within tolerance. The inverter is kept running in parallel so the input power factor of the UPS is maintained close to unity, regardless of the load power factor, as the reactive part of the load is significantly reduced in the UPS input current. In case of an interruption of the utility/mains supply, the inverter maintains the output voltage providing an uninterrupted transfer from eConversion to double conversion. The batteries are charged when the UPS is in eConversion mode and harmonics compensation is also provided.
eConversion mode can be used for the Galaxy VX UPS in the following conditions:
-
The minimum load on the UPS is 5-10%.
-
Voltage fluctuation is ≤10% versus nominal voltage (adjustable setting from 3% to 10%).
-
THDU is ≤5%.
While the UPS is in eConversion, the bypass, inverter, and load LEDs are green, and the battery and input LEDs are off.
Double Conversion (Normal Operation)
The UPS supports the load with conditioned power. Double conversion mode permanently creates a perfect sinewave at the system output, but this operation also uses more electricity.
While the UPS is in double conversion, the input, inverter, and load LEDs are green, and the battery and bypass LEDs are off.
Battery Operation
If the utility/mains supply fails, the UPS transfers to battery operation and supports the load with conditioned power from the DC source.
While the UPS system is in battery operation, the battery, inverter, and load LEDs are green, the bypass LED is off and the input LED is red.
Requested Static Bypass Operation
The UPS can be transferred to requested static bypass operation following a command from the display. During requested static bypass operation, the load is supplied from the bypass source. If a fault is detected, the UPS will transfer to double conversion (normal operation) or forced static bypass operation. If there is an interruption to the utility/mains supply during requested static bypass operation, the UPS will transfer to battery operation.
During requested static bypass, the input, bypass and output LEDs are green and the battery and inverter LEDs are off.
Forced Static Bypass Operation
The UPS is in forced static bypass operation following a command from the UPS or because the user has pressed the inverter OFF button on the UPS. During forced static bypass operation, the load is supplied from the bypass source.
During forced static bypass, the input, bypass and output LEDs are green and the battery and inverter LEDs are off or red if an alarm is present.
Maintenance Bypass Operation
for UPS Modes
When the maintenance bypass breaker MBB is closed in the external maintenance bypass cabinet, maintenance bypass panel, or third party switchgear, the UPS transfers to external maintenance bypass operation. The load is supplied with unconditioned power from the bypass source. Service and replacement can be performed on the entire UPS during external maintenance bypass operation via the maintenance bypass breaker MBB.
Static Bypass Standby Operation
Static bypass standby is only applicable to an individual UPS in a parallel system. The UPS enters static bypass standby operation if the UPS is prevented from entering forced static bypass operation and the other UPSs of the parallel system can support the load. In static bypass standby the output of the specific UPS is OFF. The UPS automatically transfers to the preferred operation mode when possible.
Inverter Standby
The UPS enters inverter standby if there is an interruption to the utility/mains supply of one UPS and the other UPS units of the parallel system can support the load with the configured redundancy level maintained. This is to avoid that the batteries are being drained in situations where it is not necessary.
ECO Mode
In ECO mode the UPS uses requested static bypass to power the load as long as the power quality is within tolerance. If a fault is detected (bypass voltage out of tolerance, output voltage out of tolerance, power interruption, etc) the UPS will transfer to double conversion (normal operation) or forced static bypass. Depending on the transfer conditions, a minimal interruption of the load supply may happen (up to 10 ms). The batteries are charged when the UPS is in ECO mode. The main advantage of ECO mode is a reduction in the consumption of electrical power compared with double conversion.
During ECO mode, the input, bypass and output LEDs are green and the battery and inverter LEDs are off.
Self-test
After start-up of the UPS system, the UPS will perform an automatic self-test. The status and progress of the self-test are indicated by the flashing LEDs on the mimic diagram.
When the self-test has been passed, the LEDs will indicate the operation mode of the UPS system.
Battery Test Mode
The UPS is in battery test mode when the UPS is performing a battery self-test or a runtime calibration.
OFF Mode
for UPS Mode
The UPS is not supplying the
load with power. The batteries are charged and the display is on.System Modes
The system operation mode indicates the output status of the complete UPS system including the switchgear and indicates which source supplies the load.
eConversion Mode
eConversion provides a combination of maximum protection and highest efficiency, that permits to reduce the electricity absorbed by the UPS by a factor three compared with double conversion. eConversion is now the generally recommended operation mode and is enabled by default in the UPS but it can be disabled via the display menu. When enabled, eConversion can be set to always active or on a set schedule configured through the display menu.
In eConversion the UPS system supplies the active part of the load through the static bypass as long as the utility/mains supply is within tolerance. The inverter is kept running in parallel so the input power factor of the UPS system is maintained close to unity, regardless of the load power factor, as the reactive part of the load is significantly reduced in the UPS system input current. In case of an interruption of the utility/mains supply, the inverter maintains the output voltage providing an uninterrupted transfer from eConversion to double conversion. The batteries are charged when the UPS system is in eConversion mode and harmonics compensation is also provided.
eConversion mode can be used for the Galaxy VX UPS system in the following conditions:
-
The minimum load on the UPSs is 5-10%.
-
Voltage fluctuation is ≤10% versus nominal voltage (adjustable setting from 3% to 10%).
-
THDU is ≤5%.
Inverter
Operation
for System Modes
In inverter operation the load is supplied by the inverters. The UPS mode can be in either double conversion (normal operation) or battery operation when the UPS system operation mode is inverter operation.
Requested Static Bypass Operation
for System
Modes
When the UPS system is in requested static bypass operation, the load is supplied from the bypass source. If a fault is detected, the UPS system will transfer to inverter operation or forced static bypass operation.
Forced Static Bypass Operation
for System Modes
The UPS system is in forced static bypass operation following a command from the UPS system or because the user has pressed the inverter OFF button on the UPSs. During forced static bypass operation, the load is supplied directly by the bypass source with unconditioned power.
Maintenance Bypass Operation
for System Modes
In maintenance bypass operation, the load is supplied directly by the bypass source with unconditioned power via the maintenance bypass breaker MBB.
ECO Mode
for System Modes
In ECO mode the UPS system uses requested static bypass to power the load as long as the power quality is within tolerance. If a fault is detected (bypass voltage out of tolerance, output voltage out of tolerance, power interruption, etc) the UPS system will transfer to double conversion (normal operation) or forced static bypass. Depending on the transfer conditions, a minimal interruption of the load supply may happen (up to 10 ms). The batteries are charged when the UPS system is in ECO mode. The main advantage of ECO mode is a reduction in the consumption of electrical power compared with double conversion.