DOCA0161ENUS-01

Chapter 3

Protection for Motor-Feeders

Introduction

A motor-feeder must satisfy the general rules of NEC standards as per Article 430. This standard defines:

  • Disconnection from power supply

  • Short-circuit protection

  • Overload protection

  • Motor control or switching

A

TeSys GV5PB / GV6PB devicen

B

Disconnection and short-circuit protection

C

Overload protection

D

Contactor

E

SDTAM thermal defect module

Characteristics Defined by UL 489 Supplement SH

TeSys GV5PB / GV6PB devices:

  • Provide protection for direct-on-line motor-feeders and star-delta motor starters (direct-on-line starting is the most widely used type of motor-feeder).

  • Integrate the basic protections (overload, short-circuit, and phase unbalance) for the motor-feeder.

  • Allow protection and coordination of the motor-feeder components that comply with the requirements of UL 489 Supplement SH.

  • Are used to create motor-feeders with two devices.

Motor Operating States

Introduction

TeSys GV5PB / GV6PB devices consider the application to be operating as soon as the 10% of Ir pickup is crossed in a positive direction by the motor current.

Two operating states are considered:

  • Startup state

  • Steady state

Startup State

The application is considered to be in startup state according to the following criteria:

  • Start: As soon as the 10% of Ir pickup is crossed in a positive direction by the motor current.

  • End: As soon as the Id pickup equals 1.5 x Ir and the td time delay equals 10 s (non-adjustable parameters).

Exceeding the 10 s time delay does not result in tripping.

NOTE: The trip unit filters the subtransient state (first current peak of approximately 20 ms on contactor closing). This current peak is not therefore taken into account when assessing whether the Id pickup has been crossed.

Steady State

The application is considered to be in steady state according to the following criteria:

  • Start: As soon as startup ends.

  • End: As soon as the 10% of Ir pickup is crossed in a negative direction by the motor current.

Operating Diagram

The following diagrams show the two cases of transition between startup and steady state:

Operating states with current I < Id before end of td Operating states with current I > Id at end of td

A

TeSys GV5PB / GV6PB devices status (green: ON position)

B

Contactor status (green: ON position)

C

Current in the motor

D

Operating state: startup state (green: active state)

E

Operating state: steady state (green: active state)

Trip Unit Description

Introduction

The trip unit is suitable for protecting motor-feeders in standard applications. The thermal trip curves are calculated for self-ventilated motors. The adjustment dials and indications are located on the front face.

Description

TeSys GV5PB trip unit

TeSys GV6PB trip unit

A

Micrologic 2.2 M/2.3 M electronic trip unit adjustment range

B

Adjustment dial for Full Load Amperes (FLA) Ir

C

Selection dial for the long-time protection time delay class

D

Adjustment dial for the short-time protection pickup Isd

E

Value of instantaneous protection pickup Ii

F

Test port

G

Phase unbalance

H

Ready LED (green)

I

Alarm LED (green)

Indication LEDs

Indication LEDs on the front of the trip unit indicate its operational state.

Indication LED Description
Green READY LED Blinks slowly when the electronic trip unit is ready to provide protection.
Red ALARM LED Overload temperature alarm LED: Shows a steady light when the thermal image of the motor exceeds 95% of the Ir setting.

The indication LEDs function for device load currents above 30 A.

Protection Functions

The following figure and table define the protection functions performed by the trip unit:

Item

Parameter

Description

Adjustable

Default setting

SDTAM activation

A

Ir

Overload or Full Load Amperes (FLA)

Yes

0.4 x In

Yes

B

Class

Trip class

Yes

10

Yes

C

Isd

Short-time protection pickup

Yes

13 x Ir

No

D

tsd

Short-time protection time delay

No

0.1 s

No

E

Ii

Instantaneous protection pickup

No

17 x In

No

C

Iunbal

Phase-unbalance protection pickup

No

30%

Yes

C

tunbal

Phase-unbalance protection time delay during startup

No

0.7 s

Yes

Phase-unbalance protection time delay in steady state

No

4 s

Yes

Each function is reviewed in detail on the following pages.

Setting the Protection

Set the overload or thermal protection pickup (Ir), the short-time protection pickup (Isd), and trip class (Class) by using the dials on the device.

Reflex Tripping

The GV6PB motor protection circuit breaker supports reflex tripping. The system of reflex protection breaks very high fault currents by mechanically tripping the device with a piston actuated directly by the pressure produced in the device from a short-circuit. This piston operates the opening mechanism, resulting in ultra-fast device tripping.

Overload or Thermal Protection (ANSI 49)

Introduction

Overload or thermal protection protects all types of motor applications against overload currents.

GV5PB  

The long-time protection is set by two dials according to the starting characteristics of the application.

The pickup setting Ir for trip unit long-time protection is expressed in amperes:

   
GV6PB  
  • This value corresponds to the operating current used in the motor application.
  • The maximum Ir setting corresponds to the trip unit rating In.

Operating Principle

Overload or thermal protection is I2t IDMT (Inverse Definite Minimum Time):

  • It incorporates the motor thermal image function.

  • It can be configured as the Ir pickup and as the trip class (Class).

Tripping curve:

Item

Parameter

Description

A

Ir

Overload or Full Load Amperes (FLA)

B

Class

Overload or thermal protection trip class

Ir Pickup Setting Value

The overload or thermal protection pickup (Ir) is set by using a multi-position dial.

The default Ir pickup setting value is 0.4 x In (minimum dial value).

The overload or thermal protection tripping range is 1.05 ˗ C1.20 x Ir according to IEC/EN 60947-4-1 standard.

The following table shows the preset values of the adjustment dial Ir in amperes for each current rating In:

Trip unit rating In (A)

150 A

250 A

400 A

600 A

Pickup Ir (A)

58 114 190 312
71 137 210 338
79 145 230 364
86 155 250 390
91 163 270 416
97 172 290 442
110 181 310 468
119 210 330 494
130 217 348 524

Trip Class Setting Value

The trip class (Class) is set by using an adjustment dial:

  • Class 5

  • Class 10 (default value)

  • Class 20

The trip class corresponds to the value of the tripping time for a current of 7.2 x Ir according to IEC/EN 60947-4-1 standard.

The following table shows the value of the tripping time depending on the current in the load for all three classes:

Current in the load

Tripping time (in seconds)

Class 5

Class 10

Class 20

1.5 x Ir

96–120

192–240

320–400

6 x Ir

5.2–6.5

10.8–13.5

20.8–26

7.2 x Ir

4–5

8–10

16–20

The precision range is -20%, + 0%.

Motor Thermal Image

The model representing heat rise and cooling in a motor load is constructed according to the algorithm for calculating the thermal demand, taking account of the iron and copper losses.

The following figure represents the limit curves for the iron and copper components calculated for class 20:

 

A

Limit temperature curve for copper

B

Limit temperature curve for iron

C

Tripping curve (low envelope)

Thermal Memory

The trip unit uses a thermal memory function to protect the motor from overheating in case of repetitive low amplitude overload conditions.

Electronic protection without thermal memory function does not protect against repetitive low amplitude overload conditions because the duration of each overload above the pickup setting is too short to cause tripping. However, each overload causes a temperature rise in the installation. The cumulative effect of successive overloads can overheat the system. The thermal memory function remembers and integrates the thermal heating caused by each pickup setting overrun. The thermal memory function remembers the thermal heating values for 20 minutes before or after tripping.

Example: Comparison of the heat rise calculation without thermal image (diagram A) and with thermal image (diagram B):

Diagram A Diagram B

0

Load control (cyclical)

1

Motor temperature

2

Thermal level calculated without thermal image (diagram A), with thermal image (diagram B)

3

Overload or thermal protection level

With thermal image, the trip unit adds the thermal effect of successive current pulses. Tripping occurs based on the actual thermal state of the motor.

Cooling Fan

The thermal image of the motor is calculated taking account of the fact that the motor is self-cooled (fan mounted on the shaft end).

Short-Time Protection (ANSI 51)

Introduction to Short Term Protection (ANSI 51)

Short-time protection protects all types of motor applications against short-circuit currents.

Short-time protection lets through motor starting currents but protects cables and motor starter devices and allows not to oversize them (useful for wide range settings devices).

Operating Principle

Short-time protection is definite time. It can be configured as the Isd pickup.

Tripping curve:

Item Function Description
A Ir Overload or thermal protection pickup
B Isd Short-time protection pickup
C tsd Short-time protection fixed time delay

Isd Pickup Setting Value

The short-time protection pickup Isd is set by using a multi-position dial.

The setting value is expressed in multiples of Ir.

Step Action
1

Set the long-time protection first: the setting pickup is Ir (A).

2

Turn the Isd adjustment dial to the value required. The setting range is 5 to 13 x Ir in steps of Ir.

3

Isd is set to Ir (A) x Isd setting.

The precision range is +/-15%.

tsd Time Delay Value

The time delay cannot be adjusted.

  • The hold time is 20 ms.

  • The maximum breaking time is 60 ms.

Instantaneous Protection (ANSI 50)

Introduction

Instantaneous protection is fixed: the pickup value is determined by the current rating In. Protection is instantaneous.

Operating Principle

Instantaneous protection is fixed: the pickup value is determined by the current rating In. Protection is instantaneous.

Tripping curve:

Item Parameter Description
E Ii Instantaneous protection pickup

Ii Pickup Value

The Ii pickup value is 15 x In (trip unit rating In corresponds to the maximum Ir setting).

The precision range is +/-15%.

The maximum breaking time is 30 ms.

Phase Unbalance Protection (ANSI 46)

Introduction

Unbalances of the motor phase currents lead to significant heat rise and braking torques that can cause premature deterioration of the motor. These effects are amplified during startup: protection must be almost immediate.

Description

Phase unbalance protection:

  • Calculates the current unbalance for each phase, compared to the average current, expressed as a percentage:

  • Compares the value of the maximum current unbalance with the Iunbal protection pickup.

The following diagram shows a maximum positive unbalance on phase 2:

If the maximum current unbalance value is higher than the phase unbalance protection Iunbal pickup, the tunbal time delay is actuated.

Phase unbalance protection cannot be deactivated.

Phase unbalance protection is activated during startup and in steady state.

Operating Principle

The phase unbalance (or phase loss) protection trips if the current unbalance exceeds the 30% fixed pickup Iunbal during a fixed tunbal time delay. The tunbal time delay differs according to the motor operating conditions:

  • Start-up phase: tunbal = 0.7 s

  • Steady state phase: tunbal = 4 s

A

Activation of startup phase.

B

Activation of protection time delay as soon as the pickup is crossed.

C

Protection tripped at the end of the fixed time delay of 0.7 s

1M

Motor current

1D

Maximum unbalance of the motor phase currents

2A

Monitoring by phase unbalance protection during startup

White: Not active

Green: Active


In steady state:

A

Activation of steady state phase.

B

Activation of protection time delay as soon as the pickup is crossed.

C

Protection tripped at the end of the fixed time delay of 4 s.

1M

Motor current

1D

Maximum unbalance of the motor phase currents

2B

Monitoring by phase unbalance protection in steady state

White: Not active

Green: Active


The phase unbalance protection does not trip if the current unbalance falls below the Iunbal pickup before the end of the fixed tunbal time delay.

A

Activation of steady state phase.

B

Activation of protection time delay as soon as the pickup is crossed.

C

Time delay is reset.

1M

Motor current

1D

Maximum unbalance of the motor phase currents

2B

Monitoring by phase unbalance protection in steady state

White: Not active

Green: Active

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.