DOCA0161ENUS-01

Maximum breaking time

Maximum time after which breaking is effective, which is when the contacts are separated and the current is completely interrupted.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.