DOCA0161ENUS-01

Ue: Rated operational voltage

A value of voltage which, combined with a rated operational current, determines the application of the equipment and to which the relevant tests and the utilisation categories are referred. For multiple equipment, it is generally stated as the voltage between phases. This is the maximum continuous voltage at which the equipment may be used.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.