DOCA0161ENUS-01

Trip class (IEC 60947-4-1)

The trip class determines the trip curve of the thermal protection device for a motor feeder. The standard defines trip classes 5, 10, 20, and 30. These classes are the maximum durations, in seconds, for motor starting with a starting current of 7.2 x Ir, where Ir is the thermal setting indicated on the motor rating plate.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.