DOCA0161ENUS-01

Minimum clearances

When installing a circuit breaker, minimum distances must be maintained between the device and panels, bars and other protection systems installed nearby. These distances, which depend on the ultimate breaking capacity, are defined by tests carried out in accordance with IEC 60947-2 standard.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.