DOCA0161ENUS-01

Ii: Instantaneous protection

This protection supplements Isd. It provokes instantaneous opening of the device. The pick-up may be adjustable or fixed (built-in). This value is always lower than the contact-repulsion level.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.